Configure a local library
Configure a custom local library to store templates of objects and variables.
TIP:
To use a custom local library on another computer, copy the folder with the library name from to the same location on another computer. Alternatively, you can use remote libraries. See Configure a remote library.
C:\Users\
UserName
\Documents\Rockwell Automation\FactoryTalk Optix\Libraries- From the main toolbar, select.Template Libraries
- InTemplate Libraries, selectand selectNew library.
- (optional) Enter a name for the library.
New library appears in
Template Libraries
.- Add templates to your library. See Create a template from an object or variable.
Provide Feedback