Display content in Project view

Display content in Project view

To display the content of interest in
Project view
, collapse nodes to see only the higher structure of the project or split
Project view
to see different areas of the information model simultaneously.
  • In the
    Project view
    toolbar, select either:
    • Navigate backward
      . Select the previously selected node or item.
    • Navigate forward
      . Select the most recently selected node or item.
  • (optional) Collapse all nodes for easier navigation. Right-click the root project node and then select
    Collapse all
    .
  • (optional) Divide
    Project view
    into two areas that you can scroll separately. Select 
    Split project view
    to divide the view. Select 
    Split project view
    again to remove the division in the view.
  • (optional) Search for content in
    Project view
    instead of having to navigate. In
    Type to search
    at the top of
    Project view
    , type the name of the item. To clear search, select
    Close
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.