- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Manage project content
Use the
Project view
pane to create and manage the contents of a project. Project view
displays a tree structure comprised of nodes. The nodes are objects and variables organized in folders. Search
Project view
to find contents without having to navigate and expand folders. Split Project view
to see multiple areas of the project simultaneously. Provide Feedback