- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Paths
You can use path shortcuts when developing your application logic.
Shortcut | Description |
---|---|
%PROJECTDIR% | A directory that contains files transferred at runtime (images, documents, and so on). Example: C:\Users\ UserName \Documents\Rockwell Automation\FactoryTalk Optix\ ProjectName |
%APPLICATIONDIR% | A directory that contains objects used at runtime, including these objects:
|
%USB ,N %where N is a number associated with the USB device. | A path to a specific USB device connected to the target device. |
Provide Feedback