Animate a graphic object

Animate a graphic object

Add and configure number, sequential, or parallel animation properties to animate an object.
  1. In
    Project view
    , select the object to animate.
  2. In
    Properties
    , at the top, select
    Add
    and then select either:
    • Number animation
      . Animate objects by changing the value to another value over specific time.
    • Sequential animation
      . Animate objects with a simple transition in the serial mode.
    • Parallel animation
      . Animate object with a simple transition in the parallel mode.
    TIP: You can also right-click a property that supports animations and select
    New
    Animation type
    .
  3. Configure animation properties. See Animation properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.