Manage graphic objects
Create, edit, move, and delete graphic object types and instances.
Any object that you create in the default
UI
folder or a subfolder of the UI
folder is automatically configured as a type. Types are available in Type view
in the UI
folder.Provide Feedback