- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Delete a graphic object
Delete a graphic object to remove the object from the project.
- InProject viewor in the editor, right-click the object to delete and selectDelete.TIP: You can also select the object to delete and press.Delete
The object is removed from the project.
Provide Feedback