- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Duplicate a graphic object
Copy and paste an object to duplicate the configuration of the object. Duplicated objects create consistency and save time when creating objects.
- InProject viewor in the editor, right-click the object to duplicate and selectCopy.TIP: You can also select the object and press.
- InProject viewor in the editor, right-click the object to contain the duplicated object and selectPaste.TIP: You can also select the object to contain the duplicated object and press.
Provide Feedback