Style sheets

Style sheets

se a Style sheet object to specify default style values displayed at runtime.
TIP: Projects can contain multiple style sheets. Multiple style sheets allow you to switch between styles. For example, you could switch between a light interface and dark interface at runtime.

Properties inheritance

Objects and object instances inherit style properties from a style sheet and object types. A property can be set at more than one level. For example, text color can be set in both the style sheet globally and on a custom
Label
object type.
Property values are resolved in this order:
  1. Instance
  2. Object type of the instance
  3. Style sheet for the object class
  4. Global style sheet
If the value of a property is set to
Default
, the property inherits the value set at a higher level, in the order above. For example, if the value of
Text color
for the instance of a
Label
object is
Default
, the color value that is set is the first value found for the same property of type, object class, or global level, in that order.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.