- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Configure a style sheet
Configure a style sheet to change the properties of the style sheet. Some style properties display a preview in the editor.
- InProject view, expand theUIfolder and select the style sheet to edit.
- InProperties, configure the properties of the style sheet.TIP: To change a property value, selectto enter a value manually, or selectto browse for and link to a tag that has the value to display. Select the box that represents the color and then inAdd Dynamic LinkSelect Color, drag to select the color and chooseSelect.
Provide Feedback