Add instances of types defined in Companion Specifications

Add instances of types defined in Companion Specifications

Add instances of types defined in
Companion Specifications
one by one to your project.
TIP: To add all nodes from a Companion Specification, see Import nodes from NodeSet. To add selected nodes from a Companion Specification, see Add an OPC UA client.
Prerequisites
(optional) Add support for custom
OPC UA Companion Specifications
to
FactoryTalk Optix Studio
. See Import Companion Specifications.
  • To add a node from Companion Specifications
  • Right-click the object or folder to contain the node and select
    New
    All
    Companion specifications
    Node-to-import
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.