- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Develop a solution for importing translations
Use OPC UA communication to import translations from another project.
Application example - client, login form

Application example - client, logged in Italian user

Application example - client, logged-in American user

NOTE:
Download a sample project:
ImportTranslations.zipPrerequisites
- Create a Server project. See Create a project.
- Create a Client project. See Create a project.
TIP:
The Client project imports data from the Server project.
- To develop the server project
- Arrange the interface elements.
- Save the project.
- To develop the client project
- Arrange the interface elements.
- Save the project.
Application design example

Select
to run server and client projects using the client emulator to test your project. To run the projects on a remote client, see Add a client device.
Run
Provide Feedback