Develop buttons for closing and shutting down
Create buttons that close the
FactoryTalk Optix Application
and shut down the host system.
IMPORTANT:
Pressing
Shut down system
immediately shuts down the host operating system
on which the FactoryTalk Optix Application
runs.For example, if you run the
FactoryTalk Optix Application
on an emulator target, pressing Shut down system
immediately shuts down Windows.Application example

TIP:
Download a sample project:
CloseApplicationShutDownSystem.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback