- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Develop a user management interface
Develop a multilingual user management solution from scratch.
TIP:
Instead of creating the user management interface from scratch, you can use the predefined widgets. For more information, from the toolbar, select
and search for
Template Libraries
User Editor
The user management interface enables you to:
- Create user accounts
- Remove user accounts
- Change the password and location of user accounts
Application example


TIP:
You can download a sample project from:
UserManagementInterface.zipPrerequisites
Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback