Main toolbar
The main toolbar at the top of
FactoryTalk Optix Studio
contains buttons used by all views in the software.Item | Description | Function |
---|---|---|
![]() | Project | Open the Start page. The Start page allows you to create, open, or close a project. |
Save | Saves the project. Select an option from the list to:
| |
![]() | Save and Commit | Save changes and commit the changes to back them up in the local repository. |
Push to remote | Push saved and committed changes to the remote repository for users to see the latest changes to the project. | |
Pull from remote | Pull the latest changes from the remote repository to see the latest changes that other users have made. | |
![]() | View History | View the history of changes to the project. Restore any commit to revert to a previous version of the project. |
Undo | Cancels the last operation. | |
Redo | Repeats the last operation. | |
Browse project files | Opens the project resource window for displaying, importing, or deleting project files such as, images, videos, documents, and certificates. | |
Template Libraries | Opens the default and custom libraries and template variables. | |
![]() | Open .NET Solution | Opens the .NET project to incorporate additional functionality using custom C# code. |
Open dashboard page | Opens a configuration dashboard to begin designing your user interface. Select the list to configure the connected device, data logging, and recipes, or manage users and groups. | |
![]() | Stop | Stops the application that is running on the client device. |
Run on Emulator | Compiles, transfers, and runs the application on the selected client device or emulator. Select a different client device from the list. | |
![]() | VPN | Opens a VPN connection. |
![]() | Remote Desktop | Opens a Remote Desktop connection. |
Provide Feedback