- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Common properties
The available properties of UI objects depend on the selected object.
NOTE:
For any property that has a non-specific numeric value, the value Auto is equal to -1. If you double-click Auto in the property, -1 appears. If you enter -1 in the property, the value displays Auto.
Property | Description | Values |
---|---|---|
Name | The name of the object. | String value. |
Type | The type of the object. | Uneditable value. |
Appearance
Property | Description | Values |
---|---|---|
Visible | Visibility of object at runtime |
|
Enabled | Whether the object allows user interaction at runtime |
|
Opacity | Transparency of the object | Numeric values from 0-100 with 0 making the object transparent. |
Blink | Allows the object to blink periodically, ignored when the object is not visible |
|
Rotation | Rotation of the object around the center point | Numeric values. Positive values indicate clockwise rotation in degrees. |
Border color | Color of the border of the object | Any selected or entered color of the linked tag. |
Fill color | Fill color of the object | Any selected or entered color of the linked tag. |
Border thickness | Thickness of the object border in pixels | Numeric value. |
Corner radius | Curvature of the corners of a rectangle in pixels | Numeric value. |
Hit test visible | Whether the user can select the object to perform event methods at runtime |
|
Move target | Determines if the object or ancestor object is movable at runtime. |
|
Size and layout
Property | Description | Values |
---|---|---|
Horizontal alignment | Align selected objects horizontally in the window |
|
Vertical alignment | Align selected objects vertically in the window |
|
Width | Width of the object | Numeric value in pixels |
Height | Height of the object | Numeric value in pixels |
Left margin | Distance, in pixels, between the left edge of the window and the left side of the object | Numeric value |
Top margin | Distance, in pixels, between the top of the window and the top of the object | Numeric value |
Right margin | Distance, in pixels, between the right edge of the window and the right side of the object | Numeric value |
Bottom margin | Distance, in pixels, between the bottom of the window and the bottom of the object | Numeric value |
Provide Feedback