- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Manage graphic objects
Create, edit, move, and delete graphic object types and instances.
Any object that you create in the default
UI
folder or a subfolder of the UI
folder is automatically configured as a type. Types are available in Type view
in the UI
folder.Provide Feedback