Duplicate a graphic object

Duplicate a graphic object

Copy and paste an object to duplicate the configuration of the object. Duplicated objects create consistency and save time when creating objects.
  1. In
    Project view
    or in the editor, right-click the object to duplicate and select
    Copy
    .
    TIP: You can also select the object and press
    Ctrl
    C
    .
  2. In
    Project view
    or in the editor, right-click the object to contain the duplicated object and select
    Paste
    .
    TIP: You can also select the object to contain the duplicated object and press
    Ctrl
    V
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.