Delete a graphic object
Delete a graphic object to remove the object from the project.
- InProject viewor in the editor, right-click the object to delete and selectDelete.TIP: You can also select the object to delete and press.Delete
The object is removed from the project.
Provide Feedback