- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Edit a data logger
Edit an existing data logger.
Prerequisites
Either:
- To edit a data logger
- From the toolbar, select.Open dashboard page
- In the central pane, selectConfigure a data logger.
- Select the data logger to edit.
- If needed, edit the loggerNameand properties.
- SelectNext.
- If there is no database for the logger, create a database:TIP: You can also right-click an existing database and selectDuplicate. Duplicating a database is useful if you want to create a database based on an existing database.
- SelectNew databaseand complete:
- Name. A name for the database.
- Type. EitherEmbeddedorODBC connection.
- SelectNext.
- Set the database properties.
- SelectNext.
- Select the database to store the logger data and selectNext.
- Select the variables that you want to log and selectNext.TIP: You can find variables by using the search field.
- SelectExit.
- (optional) Set a deadband interval.
- (optional) Store read operation codes.
- (optional) Store variable reading date and time.
Provide Feedback