- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Add instances of types defined in Companion Specifications
Add instances of types defined in
Companion Specifications
one by one to your project.
TIP:
To add all nodes from a Companion Specification, see Import nodes from NodeSet. To add selected nodes from a Companion Specification, see Add an OPC UA client.
Prerequisites
(optional) Add support for custom
OPC UA Companion Specifications
to FactoryTalk Optix Studio
. See Import Companion Specifications.- To add a node from Companion Specifications
- Right-click the object or folder to contain the node and select.
- (optional) Add optional objects to a node.
- (optional) Add collection items to a node.
Provide Feedback