- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Project nodes
Use the
Project view
pane to create and manage the contents of a project. Project view
displays a tree structure comprised of nodes. The nodes are objects and variables organized in folders. Search
Project view
to find contents without having to navigate and expand folders. Split Project view
to see multiple areas of the project simultaneously. Provide Feedback