- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Objects
An object is an element that represents a physical or non-physical component in the project. A type is a model or template object for creating instances of an object.
Create objects from
Project view
or Type view
. Change the properties of an object to change the appearance and data values displayed for that object at runtime.Provide Feedback