Develop buttons for closing and shutting down

Develop buttons for closing and shutting down

Create buttons that close the
FactoryTalk Optix Application
and shut down the host system.
IMPORTANT: Pressing
Shut down system
immediately shuts down the host operating system
on which the
FactoryTalk Optix Application
runs.
Application example
TIP:
Download a sample project:
CloseApplicationShutDownSystem.zip
Prerequisites
Application design example
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.