- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Create a button that closes the application
Create a button that closes the
FactoryTalk Optix Application
application.- InProject viewpane, right-clickMainWindow (type)and select .
- Hover-over the button, select, and enterCloseApplicationButton.
- InProperties, setTexttoClose application.
- InEvents, next toMouseClick event, selectand select .
Provide Feedback