- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Deploying projects
Compile projects to
FactoryTalk Optix Applications
and then deploy the applications to client devices.You can manage the client devices to which you deploy
FactoryTalk Optix Applications
. See Manage client devices and Deploy a FactoryTalk Optix Application.For client devices not accessible in the network, you can export
FactoryTalk Optix Applications
from FactoryTalk Optix Studio
and then import them to client devices. See Export a FactoryTalk Optix Application and Import a FactoryTalk Optix Application.Provide Feedback