- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Manage client devices
Add, remove, duplicate, and select target client devices available in the network.
The default target client device, the
Emulator
, runs locally on the development computer. The Emulator
is useful for testing FactoryTalk Optix Applications
and does not require you to install the FactoryTalk Optix Application Update Service
software.
TIP:
Rebooting the
Emulator
is not supported so that you do not accidentally reboot a device on which Windows®
is installed. Provide Feedback