- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Duplicate a client device
Duplicate a client device to configure another similar client device.
- From the main toolbar, next to, select the client dropdown menu.Run
- (optional) InClient device settings, to display only the active remote client devices, toggleActive remote devices.TIP: Refresh remote client devices by selectingRefresh.
- Select a client device.
- Select.Duplicate
Configure the duplicated client device properties.
Provide Feedback