- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Drawings
Use drawings objects to add shapes and images to your application interface.
Object | Description |
---|---|
A rectangle or square that displays at runtime. Use rectangles to create buttons or group other relevant objects. See Draw a rectangle or square. | |
An ellipse or circle that displays at runtime. Use ellipses to create buttons or group other relevant objects. See Draw an oval or circle. | |
A PNG , JPG , JPEG , BMP , or SVG image. For example, a logo. | |
An object that can have multiple image states based on the input value. Each image state may reference a different image and may have a specific opacity. If the input value does not correspond with any image state, the default value is used (first defined state). | |
An SVG Tiny 1.2 image, which properties of individual image parts can be changed at design time or runtime. For example, an alarm may trigger a particular part of an image to become red. | |
Line | A line you can draw and for which you can customize the appearance. See Draw a line. |
Polyline | A polyline and polygon that can be selected at runtime and for which you can customize the appearance. See Draw a polyline or polygon. |
Provide Feedback