Develop a constrained linear gauge

Develop a constrained linear gauge

Develop an interface that enables you to change the current value, max value, and minimum value of a variable.
NOTE:
Download a sample project:
ConstrainedLinearGauge.zip
Prerequisites
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal