- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Develop a solution that samples and stores data
Create an application that samples the value of a variable on the value change and stores that data in an embedded database.
Application example

NOTE:
Download a sample project:
SampleStoreDataValueChange.zipPrerequisites
- To develop the project
- InProject view, right-clickModeland select .
- Create a data logger with an embedded database that monitors the value change of the variable. See Add a data logger.
- Arrange the interface elements.
- Save the project.
Application design example

Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback