- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Develop a solution for importing UI
Use OPC UA communication to import the UI from another project and display the values of selected variables.
Application example (server and client)

TIP:
Download a sample project:
ImportUI.zipPrerequisites
- Create a Server project. See Create a project.
- Create a Client project. See Create a project.
TIP:
The Client project imports data from the Server project.
- To develop the server project
- Arrange the interface elements.
- Save the project.
- To develop the client project
- Arrange the interface elements.
- Save the project.
Application design example (server and client)

Select
to run server and client projects using the client emulator to test your project. To run the projects on a remote client, see Add a client device.
Run
Provide Feedback