Configure a recipes editor

Configure a recipes editor

You add a recipes editor widget by selecting it from the template libraries and editing its properties.
TIP: You can develop your own recipes management solution. For more information, see Recipes editor customization.
Prerequisites
  1. To configure a recipes editor
  2. From the toolbar, select
    Template Libraries
    .
  3. In
    Template Libraries
    :
    1. Select
      Widgets
      .
    2. Drag
      Recipes Editor
      to the
      UI
      folder in
      Project view
      .
    3. Select
      Close
      .
  4. In
    Project view
    , double-click
    RecipesEditor
    .
    The widget preview displays in the central pane.
  5. In
    Properties
    , in the
    RecipeSchema
    property, select a
    Recipe Schema
    object.
  6. In
    Project view
    , automatically configure the graphical objects and dynamic links used to assign values to ingredients at runtime by right-clicking the
    RecipesEditor
    object and selecting
    Execute Setup
    .
The ingredients list appears in the widget.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal