Develop a persistent setting specific to a user
Create a checkbox that shows or hides a clock label, which state is persistent based on the currently logged in user.
Application example
![](/content/dam/dita/en/factorytalk-optix/1-3-2/_images/UserSpecificPersistentSetting.png/_jcr_content/renditions/original)
NOTE:
Download a sample project:
UserSpecificPersistentSetting.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example
![](/content/dam/dita/en/factorytalk-optix/1-3-2/_images/UserSpecificPersistentSettingDesign.png/_jcr_content/renditions/original)
Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback