- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Develop buttons for closing and shutting down
Create buttons that close the
FactoryTalk Optix Application
and shut down the host system.
IMPORTANT:
Pressing
Shut down system
immediately shuts down the host operating system
on which the FactoryTalk Optix Application
runs.Application example

TIP:
Download a sample project:
CloseApplicationShutDownSystem.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback