View changes to a project
View the committed changes of the open project by viewing the project history.
In
represents a change that is committed to the local repository and
represents a change that is pushed to the remote repository. If you are not using version control on your computer, Configure version control to view project history in
Version history
, ![](/content/dam/dita/en/factorytalk-optix/1-3-2/_images/viewhistory.png/_jcr_content/renditions/original)
Local history
![](/content/dam/dita/en/factorytalk-optix/1-3-2/_images/remotehistory.png/_jcr_content/renditions/original)
Remote history
FactoryTalk Optix Studio
.- In the main toolbar of the open project, select.View history
- InVersion history, selectto select a commit. The changes in the commit appear highlighted. If the project is new, all content for the project is highlighted.
- Expand a highlighted object to view the changes in the object.TIP: Values that change in an object are crossed out and an arrow points to the new value.
Provide Feedback