- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
Version history contents
Version history
displays all of the changes committed to a local or remote repository for a project. Example content in 
Version history
may include:

Item | Name | Description |
---|---|---|
![]() | User initial | The first letter of the user that committed the change to the repository. |
![]() | Commit message and details | The commit with the description of the change, the date and time of the commit. Select ![]() |
![]() | Local or remote repository indicator | Icon indicates which repository contains the commit. ![]() Local history ![]() Remote history |
![]() | Change details | Indicates a change in the commit from the previous version. Expand the object to see the highlighted values that changed in the object. |
![]() | Filter | Select either All to display the entire contents of the project, or Updates to displays only changes to the selected commits. |
Provide Feedback