Deploying projects

Deploying projects

Compile projects to
FactoryTalk Optix Applications
and then deploy the applications to client devices.
You can manage the client devices to which you deploy
FactoryTalk Optix Applications
. See Manage client devices and Deploy a FactoryTalk Optix Application.
For client devices not accessible in the network, you can export
FactoryTalk Optix Applications
from
FactoryTalk Optix Studio
and then import them to client devices. See Export a FactoryTalk Optix Application and Import a FactoryTalk Optix Application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal