Import a FactoryTalk Optix Application

Import a FactoryTalk Optix Application

To deploy an exported
FactoryTalk Optix Application
, move the file to the client device and run the file.
  1. To import a
    FactoryTalk Optix Application
  2. Move the exported files to the client device.
    For example, attach the USB drive with the exported application to the client device.
  3. Run
    FactoryTalk Optix Application
    on the client system:
    • On
      Windows®
      client devices, double-click
      FTOptixRuntime.exe
      .
    • On Linux client devices, in the terminal, navigate to the
      FTOptixRuntime
      file folder and enter
      ./FTOptixRuntime
      .
    • On
      OptixPanel
      , access the web interface and then select
      Import
      under
      Load application from USB
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal