- FactoryTalk Optix Studio setup
Optional tools for IntelliSense
FactoryTalk® Optix™
allows to expand the features, properties and events of some built-in objects through IntelliSense: a NetLogic tool consisting of a C# code-completion aid made available through an editor, such as Visual Studio or Visual Studio Code.Install and Configure Visual Studio or Install and Configure Visual Studio Code on your device.
NOTE:
While you can edit an object file offline by using Notepad++, IntelliSense accessories work only on the Visual Studio or Visual Studio Code editors.
- If you are usingFactoryTalk® Optix™version 1.4.0 or later, install .NET SDKs on your device to enable the IntelliSense NetLogic installation and implementation.
- On the design device, installVisual Studio 2022 SDK, according to your device architecture.
- On the device where the application is deployed, install.NET Runtime (Windows), according to your device version.
NOTE: For instructions on how to install .NET SDK, refer to the online documentation. - To edit your object, inFactoryTalk® Optix™Studio select the
at the top of the screen.
A dialog window opens. - Select yourPreferred code editor: Visual Studio or Visual Studio Code.
- In theProject viewpanel, browse toMainWindowand add aLabel.Label1is created.
- RenameLabel1toMyLabel.
- Add a Runtime or Design Time NetLogic by selectingor depending on when you would like to use the NetLogic: at runtime or design time.A NetLogic object (for example, a NetLogic namedRuntimeNetLogic1) is created in theProject viewpanel under your project.
- Double click theRuntimeNetLogic1NetLogic.The NetLogic opens in your code editor.
- In Visual Studio or Visual Studio Code, underInsert code to be executed when the user-defined logic is started, enterLabel myLabel = Owner.Get<Label>("MyLabel");.
- PressEnterto add a new line and start typingmyLabel..IntelliSense prompts the methods, properties and events available formyLabel.by opening a dropdown menu.
- Select the method, property or event that you would like to add to yourLabelcustomization, along with the related syntax, datatype or arguments.
Provide Feedback