Failed to set Default Sample Period - Default Sample Period out of range
The
Default Sample Period
is invalid. Enter a valid Default Sample Period
with a range the is from a low of 1 microsecond to a high of 30 minutes.Provide Feedback