Move items in the Controller Organizer
Move items from their original location to a new location under a new parent item in the following ways:
- Cut and paste to move it with the mouse or the keyboard.
- Drag-and-drop the item with the mouse.
- Select multiple items to move at the same time.TIP: if FactoryTalk Security is enabled, FactoryTalk Security permissions are required to create and delete items in theController Organizerand theLogical Organizer.
For additional navigation information, see:
Provide Feedback