Add Actions for Each Step

Add Actions for Each Step

Use actions to divide a step into different functions that the step performs, such as controlling a motor, opening a valve, or placing a group of devices in a specific mode.
add_act_step
Call Out 1
Step
Call Out 2
Actions
Call Out 3
Mix
Call Out 4
Do this....
Call Out 5
...and do this
Each action uses a qualifier to determine when the action starts and stops. When specifying the actions of a step, consider if an action requires a specific qualifier.
If you want the action to
And
Then assign this qualifier
Which means
start when the step is activated
stop when the step is deactivated
N
Non-Stored
execute only once
P1
Pulse (Rising Edge)
stop before the step is deactivated
L
Time Limited
stay active until a Reset action turns off this action
S
Stored
continue for a specific time, even if the step is deactivated
SL
Stored and Time Limited
start a specific time after the step is activated (step must still be active)
stop when the step is deactivated
D
Time Delayed
stay active until a Reset action turns off this action
DS
Delayed and Stored
start a specific time after the step is activated, even if the step is deactivated before this time
stay active until a Reset action turns off this action
SD
Stored and Time Delayed
execute once when the step is activated
execute once when the step is deactivated
P
Pulse
start when the step is deactivated
execute only once
PO
Pulse (Falling Edge)
turn off (reset) one of the actions of another step:
  • S - Stored
  • DS - Delayed and Stored
  • SD - Stored and Timed Delayed
arrow_right (2)
R
Reset
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.