- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Bind properties
When a property is bound to a data item, the value of the property is specified dynamically at runtime. A data item can be a tag, an extended property of a tag, a property of a graphic element or screen, or an expression.
If a property can be bound, a
appears next to the property name when you point to it.
Binding
button 
Provide Feedback