Change a property

Change a property

Change the properties in graphic elements, instances of an Add-On Graphics, screens, popups, shortcuts, and folders. For example, change the
Security
property of a screen to limit access to it, or change the
FillColor
property of a graphic element to change the color of the item.
To change a property
  1. In the
    Toolbox,
    or on an open screen, select an item or multiple items.
  2. In the
    Properties
    window, select the
    Properties
    tab. The properties for that item are displayed in categories.
    TIP:
    Tips:
    • Select multiple items to display the common properties of the items.
    • Select multiple items of the same type in the
      Project Explorer
      to display their common properties.
  3. Expand a category to display a property and change the value of the property.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.