Properties window

Properties window

How do I open the Properties window?
On the
Menu
bar, select
View > Properties Window
.
The
Properties
window consists of several tabs that may include
Properties
,
Animations
,
Columns
,
Filters
, and
Events
. The tabs on the
Properties
window depend on the item selected. The types of items include:
  • A screen, popup, shortcut, or Add-On Graphic definition
  • An element on a screen, popup, or shortcut, or Add-On Graphic definition
  • An item in the
    Project Explorer
  • An graphic element in the
    Graphic Explorer
Each tab displays the attributes and behaviors you can configure for the selected item. The name of the selected item appears at the top of the
Properties
window.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.