- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Content reuse
Create a project using content from one or more existing
View Designer
projects. For example, assume that you use the same screen in multiple projects and now the screen requires updating. Instead of making the changes to each screen in each project, make the changes to the screen in one project and then copy it to the other projects. Or assume that you have different projects but the same users are accessing them. Configure the security access for each user in one project and then copy them to the other projects.
The ability to cut or copy and then paste content depends on the item:
Item: | Cut or copy within a project? | Cut or copy to a different project? |
Project Explorer | ||
Navigation Menu content | Yes | No |
User-Defined Screens folder | No | No |
Predefined Screens folder | No | No |
Predefined screens (excluding System Banner) | Copy to User-Defined Screens folder only; no cut | Copy to User-Defined Screens folder only; no cut |
Important: Pasting screens or popups in the Predefined Screens folder is not allowed. | ||
Images folder | No | No |
Screens with no user-defined properties | Yes | Yes |
Screens with user-defined properties | Yes | Yes |
Screens with shortcuts | Copy only; no cut | Copy only; no cut |
Popups with no user-defined properties | Yes | Yes |
Popups with user-defined properties | Yes | Yes |
Shortcuts | Yes | No |
System Banner | No | No |
Screen and popup content | ||
Graphic elements | Yes | Yes |
Images | Yes | Yes |
Drawing elements | Yes | Yes |
User-defined properties | Yes | Yes |
Controller reference | Yes | Yes |
Security Administration user account | Yes | Yes |
Table content (State Table, Color Table, Property Definition tab) | ||
Rows | Yes | Yes |
Cells | Copy only; no cut | Copy only; no cut |
Pasted content retains its appearance and behavior:
- Screens and popups paste with all of their content.
- Links to shortcuts and popups are retained.
- Navigation events are retained. Verify that the navigation works correctly.
- Graphic elements maintain their physical size and position on the screen.
- Content pasted between projects with different terminal sizes are converted using theDo not scalescaling mode.
- Position animation behavior may change when copying and pasting with projects of different terminal sizes. The animation works, but the location that it begins and ends may be different due to scaling.
Provide Feedback