- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Rename a project
Change the name of an open project. Renaming a project file does not change the project name.
To rename a project
- In theProject Explorer, right-click the project and selectRename.
- Type a new name for the project file and selectEnter.
- The name must contain only numbers, letters, and underscores.
- The name must not begin with a number, contain spaces, have more than one underscore in a row, or end with an underscore.
On the- The name must not be a reserved keyword:KeywordKeywordKeywordKeywordKeywordKeywordKeywordKeywordABSACOSACSANDASINASNATANATNBEGIN_NT_RUNGBYCASECOSDEGDEGDOELSEELSIFEND_CASEEND_FOREND_IFEND_NT_RUNGEND_REPEATEND_WHILEEXITFORFRDGOTOIFIMAGESLNLOGMODNOTOFORPROFILESRADREPEATRETURNSINSQRSQRTTANTHENTHISTOTODTRNTRUNCUNTILWHILEXOR
Standardtoolbar, selectSave.
Provide Feedback