- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Save a project
As a best practice, save a project frequently while working on it. This prevents data loss due to an unexpected power failure or other problem.
By default, projects are saved as .vpd files in the project directory <user>\My Documents\Studio 5000\Projects.
To save a project
- On theStandardtoolbar, selectSave
.
Provide Feedback