Display alarms

Display alarms

Display alarms to monitor and manage control system alarms.
View Designer
provides a default
Alarm Summary
screen,
Alarm Manager
screen, and
Alarm History
screen. Change an alarm screen or add an alarm table graphic element to a new screen to create your own alarm screen.
View Designer
requires no configuration or tag binding to display alarms on the HMI device. Use
Logix Designer
to program alarm detection instructions and create tag-based alarms in a
Logix 5000
controller.
Each controller in a
View Designer
project displays a combination of up to 4,000 tag-based or 1000 instruction-based alarms. The 5380, 5480 and 5580 Logix families of controllers support tag-based alarms. A
View Designer
project with four controllers displays a maximum of 16,000 tag-based alarms.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal